Points view (output device, sourcing)

Use the
Points
view to:
  • View a summary of the points for the output device.
  • Configure the output points for the device.
  • Enable or disable No Load Detection for an output point if applicable.
  • Diagnose a problem for an output point.
  • If supported, disable Internal Short Circuit Detection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal