Fault/Program Action view parameters

Parameter
Description
Points
Indicates the point to which the configuration applies.
Output State During Fault/Program Mode
Specifies the behavior of each output when the controller's mode changes to Program or the connection from the controller to the output device is broken. Valid values are:
  • Off
    (default)
  • On
  • Hold
This parameter is not available in Run and Remote Run modes.
WARNING:
Do not change the Fault/Program Mode values online in the
Fault/Program Action
view, on the Controller Tags, or by MSG instruction. Changes will only take effect after a power cycle.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal