Fault/Program Action view
Use this view to configure the safe state Fault and Program values that the device uses when
the controller’s mode changes to Fault or Program. Use this view to:
- Set a value for each output when the controller transitions to Program mode.
- Set a value for each output when the connection from the controller to the output device is broken after being initially established.
- Select how outputs respond if there is a communication failure in Program mode.
Provide Feedback