Points view parameters (output devices)

The
Points
view includes these parameters:
Parameter
Description
Point
Indicates the point number to which this configuration applies.
Output State During
Program Mode
Determines the behavior of each output when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored and the output behaves according to these conditions:
  • Off
    - Output is 0 or Off
  • On
    - Output is 1 or On
  • Hold
    - Output maintains last state
Output State During
Fault Mode
Determines what happens to the output of each point after a communication fault occurs and the device enters Communications Fault mode.
  • Off
    - Output is 0 or Off
  • On
    - Output is 1 or On
  • Hold
    - Output maintains last state
Fault Mode Output State
Duration
Determines the length of time the output state is held prior to transitioning to the Final Fault State.
Fault Mode Output State
Final State
Determines whether the device transitions to On or Off after the Fault Mode Output State Duration elapses. The default final state is Off. If you choose Forever for Duration, the Final State setting is ignored and the device retains its current Fault mode state.
Mode when Connection Fails in Program Mode
Determines the output action if communication fails in Program Mode.
  • Leave outputs in Program Mode State
  • Change outputs to Fault Mode State
Enable Diagnostics
Enables short circuit and open wire detection on the point when selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal