Points view (output devices)
Use the
Points
view to:- View a summary of the points properties.
- Configure the behavior of each output point when:
- a communication fault occurs and the device enters Fault mode.
- the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored, and the output behaves according to the behavior selected.
- a communication failure occurs while the controller is in Program mode.
Provide Feedback