Summary View

TCI’s harmonic passive filter with PQconnect provides tuned circuit contactor control, unit status detection, metering, waveform, and power quality data. The Filter’s PQconnect data is available via Modbus RTU, EtherNet/IP, and Bluetooth.
General
:
  • Software Version:
    Latest Filter’s PQconnect software revision
  • Filter Model:
    Production type of Harmonic Passive Filter.
  • Serial Number:
    Filter’s Serial Number found in the product’s nameplate (found of each passive filter)
  • PCB Number:
    Filter’s PQconnect PCB Number, set by Factory.
  • Rated Current:
    Current Rating of the Filter.
  • Rated Voltage:
    Voltage Rating of the Filter.
  • Rated Frequency:
    Frequency Rating of the Filter.
  • Line Voltage:
    Utility Voltage in RMS being measured.
  • Line Frequency:
    Utility Frequency in Hz being measured.
  • Line Rotation:
    Order in which the voltage waveforms of a polyphase AC source reach their respective peaks. Can be “ABC” or “ACB.”
  • Board Temperature:
    Filter’s PQconnect board temperature.
Filter Line/Load
:
  • VRMS:
    Filter’s alternating current (AC) Root Mean Square voltage.
  • THVD:
    Displays the Total Harmonic Distortion of the utility line/load voltage as a percentage.
  • IRMS:
    Filter’s alternating current (AC) Root Mean Square current
  • THID:
    Displays the Total Harmonic Distortion of the utility line/load current as a percentage.
Note:
Line/Load power values are calculated using fundamental values.
Status Detection
:Filter’s Status Alerts for the input, output and of the filter will display according to severity of the alerts. For more information about each alert/fault review the Help Page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal