Alerts Management

Alert Management Summary
The
Alert Management Table
describes and provides a means to change how the filter responds to certain status conditions and what events trigger them. All possible alert statuses that can be incurred during operation are listed in the table. Typically, a user will leave the table to its default settings but can turn off/on certain statuses, which can be helpful in some specific applications. However, suppose a status condition gets triggered during the regular operation of the filter. In that case, the “Summary” screen of the Add On Profile Status section will display the most recent fault along with a coloring coding scheme of the severity of that status. A blue status condition is considered an informational indicator; yellow status conditions are caution indicators. These active alerts should be managed as soon as possible.
Alert Event Options
Two main events can be configured for each Alert option in the list of checkboxes: "
Relay & LED
" and "
Contactor
." When the
“Relay & LED”
option is selected, the PQconnect board inside the filter will illuminate an LED and close the custom relay output, allowing the user to connect to an external device. On the other hand, choosing the
'Contactor'
option will automatically open the filter's internal contactor when the status condition is met, resulting in the removal of the tuned circuit from the filter's circuit.
Alert Status Table
Below is the list of alerts the Filter monitors and the parameters under which they are categorized (e.g., Status Line, Status Filter, Status Load). These parameters can be thought of as the generated statuses triggered by the environment in which the filter is placed.
The preferred order for listing the status detection options is defined as follows:
Priority
Alert
Alert Severity
0
Phase A Tune Phase Loss
Caution
1
Phase B Tune Phase Loss
Caution
2
Phase C Tune Phase Loss
Caution
3
Phase A Tune Current Unbal.
Caution
4
Phase B Tune Current Unbal.
Caution
5
Phase C Tune Current Unbal.
Caution
6
Phase A Tune Undercurrent
Caution
7
Phase B Tune Undercurrent
Caution
8
Phase C Tune Undercurrent
Caution
9
Phase A Tune Overcurrent
Caution
10
Phase B Tune Overcurrent
Caution
11
Phase C Tune Overcurrent
Caution
12
Under Temperature
Information
13
Over Temperature
Information
14
CPU Fault
Caution
15
Tune Reactor Thermal SW
Information
16
Reclose Limit
Information
17
NCP Fault A
Caution
18
NCP Fault B
Caution
19
Line Reactor Thermal SW
Information
32
Phase A Line Phase Loss
Information
33
Phase B Line Phase Loss
Information
34
Phase C Line Phase Loss
Information
35
Phase A Line Overvoltage
Information
36
Phase B Line Overvoltage
Information
37
Phase C Line Overvoltage
Information
38
Frequency Mismatch
Caution
39
High Voltage THD
Information
40
Phase Rotation
Information
48
Phase A Load Current Unbal.
Information
49
Phase B Load Current Unbal.
Information
50
Phase C Load Current Unbal.
Information
51
Phase A Load Overcurrent
Information
52
Phase B Load Overcurrent
Information
53
Phase C Load Overcurrent
Information
Relay Input 1 & 2
Two Input relays are available to the Filter to alert the user if the terminals J7/J8 are shorted. An external relay (not on the PQconnect) can provide a signal to the PQconnect’s “Relay Input 1” & “Relay Input 2”. The Contactor Control Mode must be set to ‘Relay” to use this feature.
External Input defines the relay as an input for the contractor if it is in relay-controlled mode. If both relays are configured as External Input, their input is treated as either or. The table below gives a general overview of Relay Input Settings options.
"
Tune Thermal SW
" and "
Line Thermal SW
" indicate that the relay is tied to a thermal sensor switch on either the tuning or mainline voltage lines. A signal from the relay in these modes will trigger the associated event in the system.
Relay Input Options
Terminals are shorted
Terminals are un-shorted
Tune Thermal SW
No Alert, Temperature is normal
Alert Triggered, Temperature is high
Line Thermal SW
No Alert, Temperature is normal
Alert Triggered, Temperature is high
Reset Command
No change
Reset Alerts & resume normal operation
External Input
Contactor instructed to Open
Contactor instructed to close
The Relay Input option "
Reset Command
" will reset the contractor back to its configured mode if it was triggered open by a fault or other means. This is the same action as pressing "
Reset Contractor
" on the Contractor Control Screen.
Save Settings
Saves any modified settings so that they will remain after a power cycle. Saving the settings will automatically open the contactor.
Reset PQconnect
An easy and effective way to power cycle the Filter’s PQconnect board. Any unsaved settings will be lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal