Checklist for the Controller System
    ✔  | System Requirements  | 
|---|---|
Are you using only the certified components for your SIL level, with the corresponding firmware release, as listed at https://rok.auto/certifications?  | |
Have you calculated the safety response time of the system for each safety function?  | |
Does the response time of the system include both the user-defined safety-task program watchdog (software watchdog) time and the safety task rate/period?  | |
Is the system response time in proper relation to the process safety time?  | |
Is the system response time in proper relation to the process safety time?  | |
Have you performed all appropriate project validation tests?  | |
If necessary, have you created a prescan routine to initialize safety critical data?  | |
Have you determined how your system can handle faults?  | |
Does each network in the safety system have a unique safety network number?  | |
Is each safety device configured with the correct safety network number?  | |
Have you generated a safety signature?  | |
Have you uploaded and recorded the safety signature for future comparison?  | |
After a download, have you verified that the safety signature in the controller matches the recorded safety signature?  | |
Do you have an alternate mechanism in place to preserve the safety integrity of the system when making online edits?  | |
Have you considered the checklists for using SIL inputs and outputs?  | 
Provide Feedback