- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
SVG Element Property
SVG element property
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
ID | ID | Selects a part of the SVG file using the ID | |
Property | Property | ||
Value | Value | Value displayed and possibly changed by the user |
Provide Feedback