- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Variable transition event
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Variable NodeID | VariableNodeId | (Inherited from VariableCondition event) | |
New value | NewValue | (Inherited from VariableCondition event) | |
Old value | OldValue | (Inherited from VariableCondition event) | |
EventId | (Inherited from BaseEventType) | ||
EventType | (Inherited from BaseEventType) | ||
SourceNode | (Inherited from BaseEventType) | ||
SourceName | (Inherited from BaseEventType) | ||
Time | (Inherited from BaseEventType) | ||
ReceiveTime | (Inherited from BaseEventType) | ||
LocalTime | (Inherited from BaseEventType) | ||
Message | (Inherited from BaseEventType) | ||
Severity | (Inherited from BaseEventType) |
Provide Feedback