Set Network Path in IntelliCENTER explorer
Use the
Set Network Path
tab to set, modify, or clear the network path.
To set Network Path in IntelliCENTER explorer
- On the explorer bar, select
Devices. - Select theIntelliCENTERtab.
- In theIntelliCENTERexplorer, right-click the lineup and selectSet Network Path.
- In theSet Network Pathtab, select a network and either paste the network path orBrowseto a path.
- SelectStart Status Monitoringto start status monitoring the lineup. All network paths must be set to start status monitoring. If you do not want to start status monitoring, selectSave and Closeto save the network paths and continue working.
- To clear a network path, use the Delete function.
- For network paths that were previously setup, theSet Network Pathtab changes to theEdit Network Pathtab.
- To communicate with the controller, Add a VPN driver.
Provide Feedback