Add a VPN driver
Follow these steps to add a VPN driver for communicating with the controller.
- Select
to open the Deploy Center. - In the Path column for a controller, select
and select Set controller path. - In the Set Device Path dialog, select
Configure Drivers. - In Available Driver Types, selectFactory Talk Remote Access (VPN).
- SelectAdd New.
- In the Change the VPN Endpoint dialog, expandEndpointsandDevices.
- Select the endpoint and selectOK.
- On the Configure VPN dialog, set the Discovery Method toBroadcast > Local Broadcast.
- SelectOKand close the Configure VPN dialog.
- On the Set Device Path dialog, right-click the endpoint and selectConnect.
- Expand the endpoint to see the available controllers.
- Select your controller and selectOK.
Provide Feedback