View panes
Toggle to view panes at a specific location in the user interface.
FactoryTalk Design Studio
retains pane location and view status when you exit and then restart FactoryTalk Design Studio
. - From theViewmenu, select the pane to view:
- Explorers. Select the explorer to appear in the left pane by default:
- Systemexplorer. View theFactoryTalk Smart Objects of your system under which to create a program and routine and the tags and parameters of theFactoryTalk Smart Object.
- Executionexplorer. View and organize the contents of a project to design a physical model of your project.
- Libraryexplorer. Move aFactoryTalk Smart Objectdefinition from theSystemexplorer to reuse theFactoryTalk Smart Objectfrom the library.
- Properties. This pane appears in the right pane by default.
- Toolbox. This pane appears in the right pane by default.
- FactoryTalk Design Studio Copilot. This pane appears in the right pane by default.
- Output. View error, warning, and information messages for the routine in your project.
- On the pane bar, toggle to view panes at the specified location:
Left panes. Displays panes last pinned to the left side.
Right panes. Displays panes last pinned to the right side.
Bottom panes. Displays panes last pinned at the bottom.TIP: To view the panes from the menu bar, selectViewand then selectLeft panes,Right panes, orBottom panes.
- (optional) To change where panes appear, Set layout.
Provide Feedback