Set layout
By default in
FactoryTalk Design Studio
, certain panes appear pinned in certain locations:- Exploreris pinned in the left pane.
- Toolbox,Properties, andFactoryTalk Design Studio Copilotappear pinned in the right pane.
- Outputappears pinned in the bottom pane.
Move other panes to these locations to customize the configuration of the user interface. View or move panes on the interface to save room, view only pertinent panes, and customize the interface.
FactoryTalk Design Studio
retains the display and position of panes after you exit and restart FactoryTalk Design Studio
.To set layout
- Drag the title bar of a pane to move the pane to a different location on the interface. Panes drop into location on the left, right, and bottom of the user interface.
- Specify the visibility of an individual pane and the pane content. On the title bar of the pane, select
to select: - Pin. Pin the pane to the current location. To unpin the pane instead, selectUnpin.
- Collapse. Hide the content of the pane. To display the content instead, selectExpand.
- Close. Close the pane.TIP: The view of unpinned panes does not toggle. Unpinned panes remain displayed on the user interface.
- To revert to the previous layout, Reset layout.
Provide Feedback