- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Default JSON subscription
Expected payload format is Default JSON. You must define a folder with variables that the Subscriber will modify with payload values.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Folder | Folder | This folder node contains variables on which the Subscriber will copy the values read from the broker | |
Topic | Topic | (Inherited from Subscription) | |
QoS | QoS | (Inherited from Subscription) |
Provide Feedback