User Interface

Use the
FactoryTalk® Design Studio
interface to create a project and arrange the user interface to depict your system. Specify which panes to view and reset the layout to the default if necessary.
FactoryTalk® Design Studio
This image shows the FactoryTalk Design Studio interface.
Interface Elements
Item
Description
Toolbar
Explorer bar
Output pane
Online pane
Toolbox
Pane bar
Properties pane

Safety Element Indicators

  • The category or class label of Safety indicates safety devices.
    Safety Device Category
  • The icon decorator indicates safety objects.
    Safety Icon Decorator
  • The
    Guardmaster®
    watermark indicates safety routines.
    Safety Routine Watermark
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal