FactoryTalk Design Studio Overview

FactoryTalk® Design Studio
is a cloud-based design environment for industrial automation systems that use the
ControlLogix®
and
CompactLogix®
platforms. Use
FactoryTalk® Design Studio
to efficiently create systems that support multiple controllers, multiple collaborating engineers in a single project, and scalable reusable content.
In
FactoryTalk® Hub
, click on the
FactoryTalk® Design Studio
tile.
TIP: A valid entitlement is required to click on the tile. See Entitlements and timed trials from the for more information.
FactoryTalk® Hub
Design applications
This image shows the FactoryTalk Hub interface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal