Create a project
For information and instructions on how to create a project for safety
applications, see
Develop Safety Applications in
.FactoryTalk Design Studio
Programming Manual, publication FTDS-PM001Create a project to build your system design. All projects are stored in a remote repository
to provide access to collaborators.
Project names must adhere to the following rules:
- The first character must be a letter.
- The subsequent characters can be letters, numbers, or underscores.
- The last character must be a letter or a number.
- The project name must be at least two characters, with a maximum length of 40 characters.
- The project name cannot end in the reserved phrasel5xconvert.
Create a project from the
Welcome
page or the File
menu.
TIP:
You can have only one project open at a time.
- Close any open project.
- Either:
- On theWelcomepage, selectNew project.
- From the menu bar, selectFile > New project.TIP: The first time you open a project in FactoryTalk Design Studio, theGetting Startedpage opens with information about features to start using FactoryTalk Design Studio. To close theGetting Startedpage, in theGetting Startedtab, select
. To reopen the Getting Startedpage at any time, in the main toolbar, select
Getting Startedfrom theHelpmenu.
- InNew project, inName, enter a unique name for the project.TIP: To share an existing project, with the open project, selectFile > Source control > Share project.New Project
- SelectCreate. FactoryTalk Design Studio creates the empty project.
Provide Feedback