Add an Unassigned I/O Device to a Safety Controller
You can add devices to the Unassigned folder and then assign devices to
a controller as the safety project develops. You can also use the Unassigned folder to move
devices between controllers.
IMPORTANT:
Unassigned safety
I/O devices do not have a Safety Network Number (SNN).
FactoryTalk®
Design Studio™
automatically generates the SNN when you assign the safety I/O device to a safety
controller.- In Devices explorer, right-click the Unassigned folder and select New device...
- In the Assign Devices To dialog, under Category filter, select Safety.
- In the Add Devices To dialog, select the devices you want to add.
- Select Continue.
- Under Pending to configure, enter the device name and slot number.TIP: Alternatively, you can assign the slot number in the module properties dialog after you assign the device. An error shows until you assign the slot number.
- Select Finish to add the devices. The devices appear in the Unassigned folder.
- Assign a safety I/O to the safety controller.
- Right-click the controller backplane and select Add device...
- In the Assign devices to dialog, select Project
- Select the safety I/O modules and select Continue.TIP: Only devices that are compatible with the controller show in the list.
- Under Pending to configure, enter the device name and slot number.TIP: Alternatively, you can assign the slot number in the module properties dialog after you assign the device. An error shows until you assign the slot number.
- Select Finish to add the devices.
The devices appear in the Devices explorer.
Provide Feedback