Controlled by Window

You can tie windows to the module outputs. You can tie a window to as many as two outputs.
You can configure a window to turn an output On or Off based on configurable count/frequency/pulse width/acceleration value designation. The state change, that is, from Off to On or On to Off, occurs in less than 10 μs.
Windows Behavior Example
IMPORTANT:
You can override the output using the output tag. See Override Outputs for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal