Override Outputs

When you configure the output mode as "Controlled by Window" or "Triggered Pulse Output", you can override the state on any module output. This practice is commonly used when troubleshooting an application or testing a control system outside normal operating conditions.
You must change the following tags to override the output state:
  • O.Outputxx.OverrideDataEn
    – Set the tag to 1 to enable the
    O.Outputxx.OverrideDataValue
    to override the output state.
  • O.Outputxx.OverrideDataValue
    – Set the tag to the desired value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal