Move Velocity

The Move Velocity command instructs the axis to move to a target velocity. The sign of the target velocity determines the direction of movement.
Tags for Move Velocity Command
Tag Name
Data Type
Description
Command Tags
O.Axisxx.Command_MoveVelocity
BOOL
Indicates that the axis is to perform the Move Velocity command.
O.Axisxx.TargetVelocity
REAL
Determines the target velocity that the axis reaches. Positive values mean that the axis moves in the forward direction. Negative values mean that the axis moves in the reverse direction.
O.Axisxx.Accel
REAL
Determines the speed's rate of change.
Status Tags
I.Axisxx.ActualVelocity
REAL
Indicates the current estimated velocity of the axis.
I.Axisxx.OnTarget
BOOL
Indicates whether the axis has reached the target speed.
I.Axisxx.CommandActive
BOOL
This tag is always set when O.Axisxx.TargetVelocity is not 0. This tag is always cleared when O.Axisxx.TargetVelocity is 0.
Move Velocity Timing Diagram
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal