Protected Operations
To maintain the secure operation of your I/O module, operations that can disrupt module
operation are restricted based on the module operating mode.
In Protection Mode, the device deactivates services that could disrupt the operation of
the device, but the device continues to function. For example, configuration operations
or firmware updates are disabled to not impact the operation of the device.
The module enters Implicit Protection Mode as soon as an I/O connection is established to
the module. The module exits Implicit Protection Mode as soon as all I/O connections to
the module are stopped.
When the device is in Implicit Protection Mode, the mode prevents the following
actions:
- Firmware update request
- Module reset request
- Connection or data format change
The following operations can be applied in Studio 5000 Logix Designer application when
the modules are in Protection Mode, but as a consequence, the I/O connections are closed
and reopened:
- Change Electronic Keying
- Change RPI
- Change Unicast/Multicast
The following operations are allowed when the modules are in Protection Mode:
- Listen-only connection requests from other controllers
- I/O channel configuration change. To apply configuration change without interrupting the I/O connections, there are two methods:
- Change configurations and apply the changes in the Module Properties dialog.
- Change configuration tag values and send a Reconfigure Module MSG to the module to apply the changes.
Provide Feedback