Time Synchronization View

The Time Synchronization view is read-only and displays the CIP Sync status information about the module when the project is online. The Time Synchronization category displays the following information:
  • CIP Sync time synchronization status
  • UTC system time
  • Grandmaster Clock information
  • Grandmaster Clock description
  • Local Clock information
Time Synchronization View Example

Grandmaster Clock Description

The Grandmaster clock description dialog provides detailed information about the grandmaster clock. To view the Grandmaster clock description, select Description in the Time Sync view.
Grandmaster Clock Description Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal