Analog HART I/O Modules

This chapter describes the analog HART I/O module types and features that are common between analog HART input and HART output modules, and how to construct a PointMax I/O system.
Analog HART I/O Module Types
I/O Type
Catalog Number
Description
Input modules
5034-IF4IH, 5034-IF4IHXT
4-channel isolated voltage/current input module with HART
It supports 4 channels that accept voltage or current input.
Output modules
5034-OF4IH, 5034-OF4IHXT
4-channel isolated voltage/current output module with HART
It supports 4 channels that produce voltage or current output.
All I/O modules support removal and insertion under power (RIUP). You must remove the RTB first and then the I/O modules.
For technical and environmental specifications details, see PointMax I/O System Specifications Technical Data, publication 5034-TD001.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal