Preface
About This Publication
This manual describes how to use PointMax™ 4-channel IO-Link
master module in Logix 5000® control systems.
Make sure that you are familiar with the following:
- Use of a controller in a Logix 5000 control system
- Use of an EtherNet/IP™ network
- Studio 5000 Logix Designer® application environment
- IO-Link terminology
If you are not familiar with them, refer to your software documentation or online
help before attempting to use this module.
Provide Feedback