Use CIP Messages to Retrieve the IO-Link Event Log
To retrieve the IO-Link event log, follow the definition of the Event Log object (class
0x41) that is defined in the CIP Specification Volume 1 and Volume 7C. See IO-Link
Interface and System Specification at io-link.com.
Byte Offset | Bit Offset | Parameter |
|---|---|---|
0 | 0…2 | Reserved |
3 | Event Location (always 1 for IO-Link master module) | |
4…5 | Event Type | |
6…7 | Event Mode | |
1…2 | — | Event Code |
3…10 | — | Timestamp (only exists when IO-Link Event Timestamp is
enabled) |
You can use either attribute 14 or 22 to retrieve the event log.
To retrieve the Event Log for an IO-Link port, use a CIP message with the following
specifications:
- Communication Path = To IO-Link master module
- Instance = Port Number + 1
Provide Feedback