Highly Integrated IO-Link
Highly integrated IO-Link is the integration of IO-Link technology into the Studio 5000® design environment. All IO-Link devices become CIP™ nodes and are configured in the same way as other CIP devices.
For example, all registered IO-Link devices have their unique identity, Add-on Profiles
(AOP), tags, and appear in the I/O configuration tree under the IO-Link bus.
IO-Link technology is a worldwide open-standard protocol that integrates sensors and
other field devices into our Connected Enterprise® by connecting
the IO-Link enabled device to an IO-Link master module. You can use it to deliver data
from smart devices directly into a control system. The flexibility of IO-Link capable
devices allows machines to operate more effectively by providing diagnostics and data
including detailed machine health status to improve uptime and increase
productivity.
The benefits of IO-Link technology include:
- A worldwide open-standard peer-to-peer serial communication protocol according to IEC 61131-9
- Forward/backward compatibility with standard sensors
- Uses the same cables as standard sensors
- Allows exchange of I/O, diagnostic, and configuration data simultaneously
The benefits of integration into the Studio 5000 Logix Designer application application
include:
- Each IO-Link device has its own independent identity and connection. You can inhibit an individual device connection.
- Add and view IO-Link devices in the I/O configuration tree.
- Each IO-Link device has an AOP and can be configured like a CIP device.
- Supports Automatic Device Configuration (ADC) and if applicable, the Data Storage feature.
- Named Configuration/Input/Output tags are created for each IO-Link device.
- Configure IO-Link devices in both offline and online mode.
- Import/Export configuration for individual IO-Link devices.
- Back up configuration data for IO-Link devices into a project file in both ADC and non-ADC (Data Storage) modes.
- Provides recovery of configuration data for IO-Link devices in both ADC and non-ADC (Data Storage) modes by restoring the device configuration that is saved in a project file to the devices.
- Ease of commissioning by cloning the configuration data to another system with the same physical setup.
Provide Feedback