Cyclic Mode
All connections work in cyclic mode, except for input event connections. In cyclic mode,
both the IO-Link master module and the IO-Link device send input data at the time that
is defined in the RPI. Similarly, the controller sends output data at the time that is
defined in the RPI.
Provide Feedback