Connections

A connection is a real-time data transfer link between the owner-controller and the module that occupies the slot that the configuration references.
During the module configuration, the connection type determines what data is exchanged between the controller and the module. When you uninhibit a module in online mode, or download the project with modules that are uninhibited to the controller, the controller attempts to establish a connection to each module.
The owner-controller monitors its connection with a module. Any break in the connection, for example, the loss of power to the PointMax I/O system, causes a fault. The Studio 5000 Logix Designer application can monitor the fault status tags to indicate when a fault occurs on a module.

Producer/Consumer Communication

PointMax I/O modules use the Producer/Consumer communication model to produce data without a controller polling them first. The modules produce the data and controllers consume it. That is, the owner-controller and controllers with a Listen Only connection to the module can consume it.
When an input module produces data, the controllers can consume the data simultaneously. Simultaneous data consumption eliminates the need for one controller to send the data to other controllers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal