Change of State Mode

For input event connections, the IO-Link master module uses Change of State (COS) mode to update the input data. New data is sent to the controller immediately when a transition occurs. When there is no change of state, the data is sent at the time that is defined in the RPI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal