Device Info View
The Device Info view displays device and status information about the device when the
project is online and lets you reset the module.
Use this view to complete the following tasks during configuration:
- Determine the identity of the device.
- Monitor the Status of the device.
- Refresh the data on the screen.
- Reset the device.
- Reset the device to Factory Defaults.

WARNING:
If
StdDirectVariableRef
or
DirectParameterOverly
is present in the device IODD, the device might not
return an error if the device does not support or cannot execute the reset
command.Provide Feedback