After Adjusting the Device Configuration
After you have adjusted your IO-Link device configuration, do the following:
- Perform Device Correlation Check and select “Use Device Values”.IMPORTANT: If ADC is enabled and the adjustments are not performed in the IO-Link master Module Properties or through the configuration tags, it is necessary to perform a Device Correlation Check and select “Use Device Values”. Otherwise the new configuration is lost when the connection is dropped and reopened for any reason.
- If the device supports Data Storage, check the Data Storage Match parameter in the Device Info view to verify if the Data Storage copy in the IO-Link master module is synchronized to the device. It may take up to a minute for the status to be updated.If the Data Storage copy is not synchronized, see Table 2 for troubleshooting steps.
Provide Feedback