Standard Output Module Operation

The controller sends data to the output module at one of the following:
  • RPI
  • After an Immediate Output (IOT) instruction is executed
IMPORTANT:
An IOT instruction sends data to the module immediately, and resets the RPI timer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal