No Load Detection

No Load Detection detects when a wire is disconnected from the output or a missing load for each output point. No Load Detection occurs only when the output point is in the Off state.
The No Load Detection feature is disabled by default. You must enable the feature in your Studio 5000 Logix Designer application project.
The
I.Ptxx.NoLoad
tag indicates the presence of a No Load condition when it is set to 1. You can monitor a module tag in your program that corresponds to the No Load Detection to check for a fault.
For the minimum load current that is supported by the module, see the PointMax I/O Systems Specifications Technical Data, publication 5034-TD001.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal