AC and DC Mode

IMPORTANT:
This feature is only applicable for 5034-OA4/XT module. This module does not support mixed AC and DC operation. All points operate in the same mode, either AC or DC, based on the module configuration.
The 5034-OA4/XT module can operate either in 120/240V AC or 240V DC.
By default the module operates in AC mode with AC power supply. You can switch to DC mode if your application requires DC output with DC power supply. You can enable DC mode by selecting the Enable DC mode checkbox on the Points View.
If the module is operating in DC mode, the module does not support field power loss detection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal