Set the Network Address
You can set the network address using one of these methods:
If the network uses 192.168.1.x, we recommend that you use the rotary switches to set the
last octet of network IP address. Valid numbers range from 001…254.
To use the rotary switches to set the IP address, turn the switches to the appropriate
numbers before you install the adapter.
The bottom switch represents the first digit in the x1 position, the middle switch
represents the middle digit, and the top switch represents the digit in the x100
position.
Provide Feedback