Assemble the PointMax I/O System

To install the PointMax I/O system, complete the following steps:
  1. EtherNet/IP adapter
    • Set the network address
    • Install the EtherNet/IP adapter
  2. Install mounting bases
    • Install the end cap
  3. Install I/O modules
  4. Install the RTB
    • Insert RTB key (optional)
  5. Install accessories (optional)
    • Add a color marker for RTB
    • Install a shield clamp
    • Install a wire holder
  6. Remove and replace adapter IP switch door (optional)
  7. Connect system power
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal