Retentivity storage
Retentivity storage enables you to retain changes made to the project at runtime
in a data store.
TIP:
You can use retentivity storage to retain information
about user-specific settings. If you change the settings at runtime, the changes persist
when you stop the
FactoryTalk Optix Application
and run it again.Default retentivity storages
Each new
FactoryTalk Optix
project has these default retentivity storage
objects:- SecurityRetentivityStorage
- Records information about users and groups added to the project.
- AlarmsRetentivityStorage
- Records information about alarms added to the project.
TIP:
Rockwell Automation
recommends
keeping the default retentivity storage objects in your projects.Custom retentivity storages
You can create multiple custom retentivity storage objects in your project.
For projects uploaded from devices, you can decide whether to retain or delete data
from retentivity storages.
Each retentivity storage object has the same properties.
You can back up and restore data of retentivity storages:
To track completed backups, use Backup Completed event in your application logic.
Retentivity storage location
The default location of the
RetentivityStorage.db
file depends
on the platform running the FactoryTalk Optix Application
.- Windows PC
- Emulation inFactoryTalk Optix Studio:C:\Users\UserName\AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\Project\ApplicationFiles
- FactoryTalk Optix Applicationdeployment:C:\Users\UserName\AppData\Local\Rockwell Automation\FactoryTalk Optix\FTOptixApplication\Projects\Project\ApplicationFiles
- Linux HMI
- /persistent/data/Rockwell Automation/FactoryTalk Optix/FTOptixApplication/Projects/Project/ApplicationFiles/
- Windows panel IPCs
- C:\Users\UserName\AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\Project\ApplicationFiles
IMPORTANT:
High Availability: This local
RetentivityStorage.db
file is used only when the project runs standalone. If you add the
HighAvailability module to the project, all retentivity storage objects,
including the default objects and any custom objects, automatically switch to
the shared cluster database instead of the local file. This change occurs when
the module is added. No manual migration or reconfiguration of individual
retentivity storage objects is required.data store
retain
Provide Feedback