Configure retentivity storage backup and restore buttons
Create buttons assigned to backup and restore methods for retentivity
storage.
If you plan to back up or restore retentivity storage with a custom NetLogic, add a
custom runtime NetLogic. See NetLogic with custom backup and restore methods and #.
- To configure retentivity storage backup and restore buttons
- InProject view, create a button.For more information about buttons, see Button.For example, create a button inMainWindow (type).
- InEvents, assign one of the following methods toMouseClickEvent:
- For backup using a built-in method:/Retentivity/RetentivityStorage/Backup
- For restore using a built-in method:/Retentivity/RetentivityStorage/Restore
- For backup using a custom NetLogic method:/NetLogic/RuntimeNetLogic/CustomBackupMethod
- For restore using a custom NetLogic method:/NetLogic/RuntimeNetLogic/CustomRestoreMethod
Where:- RetentivityStorage
- Is the retentivity storage object to back up from or restore to.
- RuntimeNetLogic
- Is the runtime NetLogic with either theDoBackuporDoRestoremethods.
- CustomBackupMethod
- The name of the custom backup method. For example,DoBackup.
- CustomRestoreMethod
- The name of the custom restore method. For example,DoRestore.
You can use the configured buttons to back up and restore data at runtime.
backup
restore
retentivity storage
event
net logic
Provide Feedback