Retentivity storage properties
Each retentivity storage object has these properties.
Property | Description |
|---|---|
Nodes | A list of project nodes with data to retain.
TIP:
A node can be a project folder, for
example, the
Model folder. |
Write delay | Specifies how often changes are saved, in milliseconds. The default value is 0 . When a change is
detected, it is saved in real time, according to technical write
times.
TIP:
The default zero value may stress the hard disk drive
if large portions of the project are retained or if values are changing often. Specifying a
longer write delay puts the project at risk of potentially losing data included in the set
delay interval.
|
Delta observer enabled | In some projects, you can make changes that are not intended to be
saved. In this case, the system deactivates change detection for
executions. If False , the retentivity storage only applies
the changes already stored and does not detect future changes.
TIP:
This property is useful if you
want to use the saved retentivity layer only to apply and restore
initial changes, without adding new ones.
|
Provide Feedback