View a device profile
View a device profile to view and edit device settings such as connections, ports, and electronic keying.
TIP:
If you are online, the profile will open in read-only. You can use the offline icon to open the offline version of the profile.
- On the explorer bar, select
Devices. - Navigate to the device and double click or right-click, then selectOpen device properties.
The profile opens as a new tab in the workspace.
TIP:
You can also open the profile from the
Device list
.Provide Feedback