Supported Devices
FactoryTalk®
Design Studio™
is a web-based design environment for industrial
automation systems that use the ControlLogix®
and CompactLogix®
platforms. See in the Supported devices section of the FactoryTalk Design Studio Online Help for a complete
list of supported industrial automation devices.
For information on supported safety devices, see
Develop Safety Applications in
.FactoryTalk Design Studio
Programming Manual, publication FTDS-PM001
IMPORTANT:
IntelliCENTER®
provides support for additional devices, but these
devices currently cannot be added to a deployable control system.
Provide Feedback