Test the Application Program

This step consists of any combination of Run and Program modes, offline edits, deploy, and informal testing that is required to get an application to run properly in preparation for the project validation test.
As part of this step, generate the Safety Confirmation Report to review and confirm that the safety-related parameters are correct in the safety controller. See Confirm the Project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal