Checklist to Develop a Safety Application Program

Use the following checklist to help maintain safety when you create or modify a safety application program.
System Requirements
Were the programming guidelines followed during the creation of the safety application program?
Does the safety application program contain only a ladder diagram?
Does the safety application program contain only safety instructions?
Does the safety application program clearly differentiate between safety and standard tags?
Are only safety tags used for safety routines?
Have you verified that safety routines do not attempt to read from or write to standard tags?
Is each safety output tag correctly configured and connected to a physical output channel?
Have you defined the process parameters that the fault routines monitor?
Did you measure potential alarm bursts during system commissioning and change the project if measured scan times are not acceptable?
Has an independent safety reviewer reviewed the program, if necessary?
Has the review been documented and signed?
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal