Checklists for Safety Applications
Checklists for safety applications are required to plan, program, and start a safety application. Use the checklists as planning guides and during project validation testing. When you use the checklists as planning guides, they can be saved as a record of the plan.
The checklists provide a sample of safety considerations and are not intended to be a complete list of items to verify. Your particular safety application can have additional safety requirements.
IMPORTANT:
When the safety controller is in Run or Program
mode and you have not validated the application program, you are responsible for maintaining
safe conditions.
TIP:
Make copies of the checklists to keep for future use.
Provide Feedback