Checklist for the Controller System
✔ | System Requirements |
|---|---|
Are you using only the certified components for your SIL level, with the corresponding firmware release, as listed at https://rok.auto/certifications? | |
Have you calculated the safety response time of the system for each safety function? | |
Does the response time of the system include both the user-defined safety-task program watchdog (software watchdog) time and the safety task rate/period? | |
Is the system response time in proper relation to the process safety time? | |
Have probability (PFD/PFH) values been calculated for each safety function? | |
Have you performed all appropriate project validation tests? | |
If necessary, have you created a prescan routine to initialize safety critical data? | |
Have you determined how your system can handle faults? | |
Does each network in the safety system have a unique safety network number? | |
Is each safety device configured with the correct safety network number? | |
Have you generated a safety signature? | |
Have you uploaded and recorded the safety signature for future comparison? | |
After a download, have you verified that the safety signature in the controller matches the recorded safety signature? | |
Do you have an alternate mechanism in place to preserve the safety integrity of the system when making online edits? | |
Have you considered the checklists for using SIL inputs and outputs? |
Provide Feedback