Push Button Configuration - Peer Commands View
The Peer Command view lets you configure as many as seven peer control commands per device. To access the Peer Command View from the navigation pane the device Operating Mode must be configured to Peer Mode.
You can configure peer commands for only the illuminated push buttons; the non-illuminated push buttons do not support peer commands.
Push Button Peer Commands

From this view, you can add, edit, or delete peer commands. For more information on device-specific parameters, see Peer Commands.
Provide Feedback