Create a button that shuts down the host system
    Add a button that shuts down the host operating system on which the 
FactoryTalk Optix Application
 runs.
     IMPORTANT: 
    Pressing 
Shut down system
 immediately shuts down the host operating system
 on which the FactoryTalk Optix Application
 runs.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enter ShutDownSystemButton. ShutDownSystemButton.
- InProperties, setTexttoSHUT DOWN HOST SYSTEM.
- InEvents, next toMouseClick event, selectand select . 
Provide Feedback