Develop buttons for closing and shutting down
    Create buttons that close the 
FactoryTalk Optix Application
 and shut down the host system.
     IMPORTANT: 
    Pressing 
Shut down system
 immediately shuts down the host operating system
 on which the FactoryTalk Optix Application
 runs.Application example

     TIP: 
    
Download a sample project:
 CloseApplicationShutDownSystem.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback